Associate III
Oct 9, 2013 1:35 PM UTC
Question
stm32f429 Disco direct to VGA Monitor
- 7 replies
- 2842 views
Posted on October 09, 2013 at 15:35
Hello :)
I just remove the LCD from one of my board and made a R2R Resistor DAC connected to the LCD dedicated pin. The only pins you need are the 3 x 6bits colors , the vsync , hsync and GND. After some changes in one of the examples source from ST i was able to get a picture to my VGA Monitor ;) I just don't have the correct timing for view 640 x 480 picture , the monitor report me a 800 x 600 resolution with 31.4Khz Horizontal and 52.3Hz refresh time ... Hmmm I probably don't understand correctly the data-sheet/app note about the timing. Or i put wrong parameter for sync time + bach porch etc ... For those who want try i attach the source to put in the \Projects\Peripheral_Examples\ directory and the R2R Schematic i do for this test. If someone get the correct timing setup for 640 x 480 resolution i will be happy to get it ;) It's allot more comfortable to play with a big monitor , just no touch screen here , next step is to use a USB KB + Mouse ... he he he Cheers. PS : i compiled this with Keil.. #stm32f429-disco-vga-monitor #32f429-disco-vga-monitor-image #vga-disco-take-it #instead-of-desoldering-the-lcd