Sending large amounts of data over SPWF01SA
Hi.
So I'm trying to send large amount of data to server (~200kB). I can send and receive smallish amounts ok (<2k), however at 3k the send fails. I'm sending data in 1000byte blobs to respect the 1021byte limit in the socket code.
I've added delays and tried smaller sends also, but no luck so far. I coudn't find any applicaple callback to syncronize fe 2k transfers.
How should I handle this sort of situation?
+WIND:1:Poweron (170111-665d284-SPWF01S)
+WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2016 STMicroelectronics, Inc. Al.+WIND:3:Watchdog Running +WIND:0:Console active +WIND:32:WiFi Hardware Started+WIND:2:Reset
+WIND:1:Poweron (170111-665d284-SPWF01S) +WIND:13:ST SPWF01SA1 IWM: Copyright (c) 2012-2016 STMicroelectronics, Inc. Al.+WIND:3:Watchdog Running +WIND:0:Console active +WIND:46:WPA: Crunching PSK...+WIND:32:WiFi Hardware Started
+WIND:21:WiFi Scanning +WIND:35:WiFi Scan Complete (0x0) +WIND:19:WiFi Join:xx.xx.xx.xx.xx.xx +WIND:25:WiFi Association with 'XXXX' successful +WIND:51:WPA Handshake Complete +WIND:24:WiFi Up:192.168.0.100>>Socket Open OK
>>Socket ID: 0Writing 1000 bytes to socket, left 128825
<<OK >>Socket Write OK Writing 1000 bytes to socket, left 127825 <<OK >>Socket Write OK Writing 1000 bytes to socket, left 126825 >>Socket Write FAIL +WIND:55:Pending Data:0:ENC +WIND:58:Socket Closed:0Reached SockON_Data_Length
Data Receive Callback... AT+S.SOCKR=0,313 HTTP/1.1 400 Bad Request Server: Server Date: Wed, 26 Apr 2017 12:29:29 GMT Content-Type: text/html Content-Length: 167 Connection: closeAs the server reponds with the bad request something is sent.