Skip to main content
Mark Shoe
Associate III
January 17, 2018
Question

Backup SRAM using CubeMX

  • January 17, 2018
  • 3 replies
  • 3353 views
Posted on January 17, 2018 at 11:30

The STM32F4 has 4 Kbytes of backup SRAM.

They seems not to be accesable at a certain adress

The HAL lib has also a driver for it. But the functions are not enabled default. 

The library stm32f4xx_hal_sram is needed for the functions. There are even examples in the example directory.

But how to tell CubeMX to include these libraries, i can include myself but they are gone when a new project is generated again.

    This topic has been closed for replies.

    3 replies

    Mark Shoe
    Mark ShoeAuthor
    Associate III
    January 18, 2018
    Posted on January 18, 2018 at 14:17

    Not that hard after all:

    sram_t *sram = (uint32_t *) BKPSRAM;

    and not sure if needed:

    __BKPSRAM_CLK_ENABLE();

    HAL_PWR_EnableBkUpAccess();

    Varadharajan V
    Associate III
    March 5, 2018
    Posted on March 05, 2018 at 08:19

    It would be fine if cubemx has facility to enable and will generate all the required config like RTC Init

    Other wise we have to add the code in between USER Code Begin and User Code End so that Cubemx will not erase on next time same project is generated

    But for each project we need to do this other wise Backup SRAM wont be enabled and our code will fail in field

    I'm using this the following code inside HAL_RTC_MspInit() function after RTC Enable

    void HAL_RTC_MspInit(RTC_HandleTypeDef* rtcHandle)

    {

    if(rtcHandle->Instance==RTC)

    {

    /* USER CODE BEGIN RTC_MspInit 0 */

    /* USER CODE END RTC_MspInit 0 */

    /* RTC clock enable */

    __HAL_RCC_RTC_ENABLE();

    /* USER CODE BEGIN RTC_MspInit 1 */

    __HAL_RCC_BKPSRAM_CLK_ENABLE(); // additional code for Backup RAM enable

    HAL_PWR_EnableBkUpAccess(); 

    // additional code for Backup RAM enable

    HAL_PWREx_EnableBkUpReg(); 

    // additional code for Backup RAM enable

    /* USER CODE END RTC_MspInit 1 */

    }

    }

    after adding those codes, then we can use like non volatile area otherwise its become volatile

    Varadharajan V
    Associate III
    March 5, 2018
    Posted on March 05, 2018 at 08:20

    Better cubemx developers consider this and can provide facility inside RTC config dialog