Senior III
September 9, 2017
Solved
STM32F769I-DISCO LCD RTOS LwIP : screen corrupted [solved]
- September 9, 2017
- 2 replies
- 945 views
Posted on September 09, 2017 at 20:40
Hello.
Based on the HAL example >Applications>Display>LCD_PicturesFromSDCard I converted
this into a CubeMX (V1.7.0) project, which works fine. Adding FreeRTOS works as well.
But if I add LwIP (just adding) sometimes the image is not shown properly.
Parts of the image is corrupted on the screen.
Regardless if DHCP/static and memory settings for LwIP and FreeRTOS.
It does occur i.e. after every 6-20th image loading. There is no rule.
Why is it a problem to use LwIP in this case?
Thank you for every hint.