Skip to main content
Christoph Eschenbach
Associate III
January 26, 2017
Question

Training/Tutorial USB-UART for STM32F4?

  • January 26, 2017
  • 1 reply
  • 554 views
Posted on January 26, 2017 at 18:24

Hello there,

Im working with nucleo144F429ZI and i want to implement a USB CDC VCP Device for Tx/Rx-Data over the USER USB.

I already managed to get the CubeMX generated Sourcecode to run on the board... Sometimes.

With FreeRTOS I havent found a solution to get it work for now.

But still I miss the basic understanding what the libary really does. So its hard to find the problem when an error occurs.

And the CDC_Standalone Application for other boards arent really helpfull to understand what really is happening inside.

So can you please help me find a good starting point to get the knowladge to configure and use the USB CDC Libaries?

Any Trainings or Tutorials?(dont need to be for free)

(Read only Datasheets is a option but not the fastest one)

Thanks

Christoph

    This topic has been closed for replies.

    1 reply

    ST Technical Moderator
    January 27, 2017
    Posted on January 27, 2017 at 18:46

    Hi

    Eschenbach.Christoph

    ,

    May this

    help youand giveyou general guidelines on USB CDC.

    For more details, refer to the user manual UM1734 that explains more the use of STM32Cube USB device library.

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks