Skip to main content
ter
Associate
March 1, 2013
Question

STM32F2 LSE RTC crystal issue: Can anyone help?

Posted on March 01, 2013 at 13:45

Hello

We use the STM32F2 for a project and have problems with the LSE crystal.

We use a Citizen CMR200T crystal (32.768kHz, CL=6pF, Farnell Nr.

1652560

) wich has a gain margin of 6.1 (according to the ST application note AN2867) and therefore is suitable.

It worked fine with STM32F205VGT6 Ref Y, now we changed to Ref X and the frequency shifts about 40ppm! There are no information about changes made from Ref Y to Ref X (despite other bootloader version).

With uC Ref Y: f=32.7679kHz (-3ppm)

With uC Ref X: f=32.7694kHz (+43ppm)

The measurement are made with the same layout, crystal and CL1/CL1 of 4.7pF, only the uC has changed. The frequency is measured at PA8 which outputs the clock trough microcontroller clock output (MCO1).

Can anyone help? How can we build a accurate RTC when the frequency shifts from uC to uC?

Regards,

Timon

#stm32f2-lse-rtc-crystal-ref-x-y
This topic has been closed for replies.

2 replies

hatem_ch
Associate
April 5, 2013
Posted on April 05, 2013 at 21:14

Hello,

Y

ou may refer to the PIL MMS-MIC/12/7477 document published on ST web-site.

It mentions clearly that LSE’s transconductance was decreased in rev X die compared to rev Y die.

I think this is most probably the reason behind the observed drift in oscillation between two boards populated with different chips.

Ciao

Tesla DeLorean
Guru
April 5, 2013
Posted on April 05, 2013 at 21:32

Interestingly there is a single Google hit on this document, and it's not on ST's site. Chance of someone stumbling upon it are pretty low.

http://www.anglia.com/registration/pcn_ptn/docs/pcn/PIL%20MMS-MIC_12_7477.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..