Skip to main content
taraben
Associate III
May 26, 2015
Question

CubeMX USB CDC wrong buffer handling?

  • May 26, 2015
  • 0 replies
  • 500 views
Posted on May 26, 2015 at 22:13

Hello, in my earlier post I asked abouot buffer handling.

I investigated any further and found one potential error and one unused buffer.

1) buffer overflow

in file usbd_cdc_if.c

&sharpdefine APP_RX_DATA_SIZE  4

...

uint8_t UserRxBufferFS[APP_RX_DATA_SIZE];

...

static int8_t CDC_Init_FS(void)

{

...

  USBD_CDC_SetRxBuffer(hUsbDevice_0, UserRxBufferFS);

...

}

@see USBD_CDC_SetRxBuffer doesn't take any length information

in file usbd_cdc.c this buffer is used in function:

static uint8_t  USBD_CDC_Init (USBD_HandleTypeDef *pdev,

                               uint8_t cfgidx)

{

...

      USBD_LL_PrepareReceive(pdev,

                             CDC_OUT_EP,

                             hcdc->RxBuffer,

                             CDC_DATA_HS_OUT_PACKET_SIZE);

...

}

So that means for safe operation the length of UserRxBufferFS must be minimum CDC_DATA_HS_OUT_PACKET_SIZE size.

2) unused buffer

in file usbd_cdc_if.c

&sharpdefine APP_TX_DATA_SIZE  4

...

uint8_t UserTxBufferFS[APP_TX_DATA_SIZE];

...

static int8_t CDC_Init_FS(void)

{

...

  USBD_CDC_SetTxBuffer(hUsbDevice_0, UserTxBufferFS, 0);

...

}

This buffer is never used anywhere else.

The transmit code uses the buffer the user gives to the function.

The buffer UserTxBufferFS is not needed here and misleading.

Am I right?

Best regards, Adib.

#cdc #stm32f4 #usb #vcp
This topic has been closed for replies.