Solved
Stm32l4 1.9.0 - FatFs naming problem
Posted on October 11, 2017 at 12:26
Hi,
I am using package Stm32l4 1.9.0 package on Linux with Stm32CubeMX to generate workbench project.
It seems there is naming problem, since folder in downloaded repository is named
'STM32Cube_FW_L4_V1.9.0/Middlewares/Third_Party/FatFS'while it should be
'STM32Cube_FW_L4_V1.9.0/Middlewares/Third_Party/FatFs'This causes problem during build and code generation. Repository was updated using CubeMX.
Can somebody replicate this, or is something wrong with my configuration?I hope i am not duplicating this issue.
Best Regards, Miha