Question
ili9163 spi LCD Help Please!
Posted on February 17, 2015 at 12:00
Hi guys , I wrote this simple code based on the ili9163 documentation and what what i found online of the arduino library writen for the same display , yet all what i was able to do is get the Background LED to light up the panel , nothing diplaying apart from that , here is my code:
#include <stm32f4xx.h>#include <stm32f4xx_adc.h>#include <stm32f4xx_gpio.h>#include <stm32f4xx_rcc.h>#include <stm32f4xx_spi.h>#define CSPin GPIO_Pin_1#define ResPin GPIO_Pin_2#define AOPin GPIO_Pin_4#define DatPin GPIO_Pin_5#define ClkPin GPIO_Pin_3#define VCCPin GPIO_Pin_6#define BLPin GPIO_Pin_7#define DatPS GPIO_PinSource5#define ClkPS GPIO_PinSource3#define Red 0x8000GPIO_InitTypeDef GP_InitDef;SPI_InitTypeDef SPI_InitDef;void initGPIO(){ RCC->AHB1ENR |= RCC_AHB1Periph_GPIOB; // Clock enable for GPIOB. GP_InitDef.GPIO_Pin = CSPin | ResPin | AOPin | BLPin | VCCPin; GP_InitDef.GPIO_Mode = GPIO_Mode_OUT; GP_InitDef.GPIO_OType = GPIO_OType_PP; GP_InitDef.GPIO_PuPd = GPIO_PuPd_NOPULL; GP_InitDef.GPIO_Speed = GPIO_Speed_25MHz; GPIO_Init(GPIOB, &GP_InitDef); GP_InitDef.GPIO_Pin = DatPin | ClkPin; GP_InitDef.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOB, &GP_InitDef); GPIO_PinAFConfig(GPIOB, ClkPS, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOB, DatPS, GPIO_AF_SPI3);}void initSPI3() { // Initialize SPI3. SPI_InitDef.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_2; SPI_InitDef.SPI_CPHA = SPI_CPHA_1Edge; SPI_InitDef.SPI_CPOL = SPI_CPOL_Low; SPI_InitDef.SPI_DataSize = SPI_DataSize_8b; SPI_InitDef.SPI_FirstBit = SPI_FirstBit_MSB; SPI_InitDef.SPI_Mode = SPI_Mode_Master; SPI_InitDef.SPI_NSS = SPI_NSS_Soft; SPI_Init(SPI3, &SPI_InitDef); SPI_Cmd(SPI3, ENABLE);}void writeCommand(uint16_t command){ GPIO_ResetBits(GPIOB, AOPin); // Set A0 D/C pin LOW for command select. SPI_I2S_SendData(SPI3, command); while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_BSY) == SET);}void writeData(uint16_t data){ GPIO_SetBits(GPIOB, AOPin); // Set A0 D/C pin LOW for data select. SPI_I2S_SendData(SPI3, data); while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_BSY) == SET);}void writeData16(uint16_t data){ GPIO_SetBits(GPIOB, AOPin); // Set A0 D/C pin LOW for data select. SPI_I2S_SendData(SPI3, data>>8); while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_BSY) == SET); SPI_I2S_SendData(SPI3, data); while(SPI_I2S_GetFlagStatus(SPI3, SPI_I2S_FLAG_BSY) == SET);}void setCoordinates(){ writeCommand(0x2A); writeData(0x00); writeData(05); writeData(0x00); writeData(50); writeCommand(0x2B); writeData(0x00); writeData(32); writeData(0x00); writeData(32+50); writeCommand(0x2C);}int main(void){ int index; initGPIO(); initSPI3(); GPIO_SetBits(GPIOB, BLPin); // Set The background LED Pin high. // GPIO_ResetBits(GPIOB, ResPin); for (index = 0; index < 50000; index++); GPIO_SetBits(GPIOB, ResPin); for (index = 0; index < 50000; index++); GPIO_ResetBits(GPIOB, CSPin); for (index = 0; index < 50000; index++); //Start The LCD initializing. writeCommand(0x01); //Software reset for (index = 0; index < 50000; index++); writeCommand(0x11); // Exit Sleep for (index = 0; index < 10000; index++); writeCommand(0x26); //Set default gamma writeData(0x04); for (index = 0; index < 5000; index++); writeCommand(0xC0); //Set Power Control 1 writeData(0x1F); for (index = 0; index < 5000; index++); writeCommand(0xC1); //Set Power Control 2 writeData(0x00); for (index = 0; index < 5000; index++); writeCommand(0xC2); //Set Power Control 3 writeData(0x00); writeData(0x07); for (index = 0; index < 5000; index++); writeCommand(0xC3); //Set Power Control 4 (Idle mode) writeData(0x00); writeData(0x07); for (index = 0; index < 5000; index++); writeCommand(0xC5); //Set VCom Control 1 writeData(0x24); // VComH = 3v writeData(0xC8); // VComL = 0v for (index = 0; index < 5000; index++); writeCommand(0x38); //Idle mode off for (index = 0; index < 5000; index++); writeCommand(0x3A); //Set pixel mode writeData(0x05); for (index = 0; index < 5000; index++); writeCommand(0x36); //Set Memory access mode writeData(0x08); for (index = 0; index < 5000; index++); writeCommand(0x29); //Display on for (index = 0; index < 5000; index++); writeCommand(0x2C);//Memory Write for (index = 0; index < 5000; index++); //Display Something int px; setCoordinates(); for (px=0;px < 132; px++){ writeData16(Red); } return 0;}Any idea what Am I doing wrong ?? I appreciate it !!!