Question
IDW04A1 missing cs on CN5
Posted on October 01, 2017 at 17:44
I wish to connect an IDW04a1 Board to the Discovery kit for IOT node (B-L475E-IOT01A) to replace the Inventek WiFi module with a SPWF04SA WiFi module. It appears that the NSS/nCS/WAKEUP* signal is not routed correctly to CN5-Pin3 from Pin9 of the SPWF04SA module.In fact R33 is not mounted. The signal is routed to GPIO1 but that signal does not go to CN5.
Also, the MISO signal from SPWF04SA-Pin6 is routed to CN5-Pin5 and not CN5-Pin1.
Table 10 in UM2183 appears incorrect for the MISO and NSS signals.
Has anyone else noticed these issues?