Skip to main content
shasha liu
Associate
February 10, 2017
Question

STM32 how to use VREF to Calculate the actual VDDA value

  • February 10, 2017
  • 3 replies
  • 4336 views
Posted on February 10, 2017 at 04:34

I am using the STM32 ADC to caputure outer voltage , while the requirement to  ADC accuracy is not very high. So I decided to use the VDDA as the reference voltage. BUT  the actually vdd added to the mcu exist deviation from each others. Is there any way to get the acutal vdda after reset.?

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    February 10, 2017
    Posted on February 10, 2017 at 05:40

    Most STM32 parts also provide a VREFINT which is an internal 1.25V reference you can sample and use to compute the VREF+/VDDA voltages.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    shasha liu
    Associate
    February 10, 2017
    Posted on February 10, 2017 at 09:32

    Thanks for your replay. 0690X00000606IUQAY.png

    I still have questions about how to get the VRETINT_CAL mentioned in the datasheet.

    thanks

    Tesla DeLorean
    Guru
    February 10, 2017
    Posted on February 10, 2017 at 15:15

    What STM32 specifically are you using they make hundreds of parts in dozen of families, it's like saying you drive a Ford.

    The Reference Manual should provide the ROM/OTP address of the memory location holding the VREFINT_CAL value.

    I'd start by assuming the voltage is 1.25V, and scaling back up to what a 4095 value would represent based on the reading for VREFINT, and see how close that is to the voltage you can measure with a volt-meter.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..