Skip to main content
Dick Lin
Senior
June 20, 2018
Question

STM32L496ZG flash program issue

  • June 20, 2018
  • 10 replies
  • 1893 views
Posted on June 21, 2018 at 00:57

Hi,

I am working on STM32 flash program using a sample program from V1.11. The program is pretty straight forward. Erase ADDR_FLASH_PAGE_16 to ADDR_FLASH_PAGE_255 then program.

The program stuck in HardFault_Handler doing HAL_FLASHEx_Erase in the first page erase FLASH_PageErase(page_index, pEraseInit->Banks);

HAL_FLASH_Program()

 also failed on FLASH_Program_DoubleWord().

Anyone experienced same issue? Doesn't this supposed to be working without any changes? 

Thx

STM32Cube_FW_L4_V1.11.0\Projects\NUCLEO-L496ZG\Examples\FLASH\FLASH_EraseProgram

if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError) != HAL_OK)

{

while (1)

{

BSP_LED_On(LED3);

}

}

Address = FLASH_USER_START_ADDR;

while (Address < FLASH_USER_END_ADDR)

{

if (HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, Address, DATA_64) == HAL_OK)

{

Address = Address + 8;

}

else

{

/* Error occurred while writing data in Flash memory.

User can add here some code to deal with this error */

while (1)

{

BSP_LED_On(LED3);

}

}

}

HAL_FLASH_Lock();

Address = FLASH_USER_START_ADDR;

MemoryProgramStatus = 0x0;

while (Address < FLASH_USER_END_ADDR)

{

data32 = *(__IO uint32_t *)Address;

if (data32 != DATA_32)

{

MemoryProgramStatus++;

}

Address = Address + 4;

}

/*Check if there is an issue to program data*/

if (MemoryProgramStatus == 0)

{

/* No error detected. Switch on LED1*/

BSP_LED_On(LED1);

}

else

{

/* Error detected. Switch on LED2*/

BSP_LED_On(LED2);

}
    This topic has been closed for replies.

    10 replies

    Tesla DeLorean
    Guru
    June 20, 2018
    Posted on June 21, 2018 at 01:11

    >>Doesn't this supposed to be working without any changes? 

    How large is the executable image your tool chain is generating? More than 16KB perhaps?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Dick Lin
    Dick LinAuthor
    Senior
    June 21, 2018
    Posted on June 21, 2018 at 01:20

    The .elf file is pretty big - 1883 KB. What's the limit of the board?

    Dick Lin
    Dick LinAuthor
    Senior
    June 21, 2018
    Posted on June 21, 2018 at 01:44

    Why the flash HAL function failure has anything to do with code size?