stmCubeMx for STM32F7xx cpu ethernet function low_level_init not correct i think
static
voidlow_level_init(
structnetif
*netif)
{
uint32_t
regvalue = 0;
HAL_StatusTypeDef
hal_eth_init_status;
/*
Init
ETH */uint8_t
MACAddr[6] ;
heth.
Instance
= ETH;
heth.
Init
.
AutoNegotiation
= ETH_AUTONEGOTIATION_ENABLE;
heth.
Init
.
PhyAddress
= LAN8742A_PHY_ADDRESS;
MACAddr[0] = 0x00;
MACAddr[1] = 0x80;
MACAddr[2] = 0xE1;
MACAddr[3] = 0x00;
MACAddr[4] = 0x00;
MACAddr[5] = 0x00;
heth.
Init
.
MACAddr
= &MACAddr[0];
heth.
Init
.
RxMode
= ETH_RXINTERRUPT_MODE;
heth.
Init
.
ChecksumMode
= ETH_CHECKSUM_BY_HARDWARE;
heth.
Init
.
MediaInterface
= ETH_MEDIA_INTERFACE_RMII;
heth.Init.MACAddr is a pointer to the MACAddr. but when i leave this funtion the pointer is not pointing to a defined
memory space. It is later on in the program not possible to get the MacAddr info form
heth.Init.MACAddr. The pointer must point to a MACAddr that is available all the time the program is running.