Skip to main content
marc Georgin
Associate
January 4, 2017
Question

SPWF01 : can't connect to the mini AP

  • January 4, 2017
  • 17 replies
  • 2791 views
Posted on January 04, 2017 at 09:52

Hello,

I'am using this module to connecte my borad to Internet. 

This module can create a mini AP so a user can connect its laptaop or smartphone to the SPWF01 and configure the WIFI connexion (SSID and pass).

I have no problème to connect to the mini AP with an old WIKO smartphone but I can't connect with a newer smartphone (Huawei P9 lite).

I have also discover a weird thing : If I first connect anything (old WIKO or laptop) to the mini AP, and then try with the P9 lite, it can connect to the mini AP.

thanks for your help.

Marc G

    This topic has been closed for replies.

    17 replies

    Gerardo GALLUCCI
    ST Employee
    January 5, 2017
    Posted on January 05, 2017 at 16:18

    Hi,

    which version are you using?

    Regards

    Jerry

    marc Georgin
    Associate
    January 9, 2017
    Posted on January 09, 2017 at 11:01

    Hello,

    thanks for your help, the version of the firmware of the SPWF01 is 3.4.

    regards,

    Marc

    Gerardo GALLUCCI
    ST Employee
    January 9, 2017
    Posted on January 09, 2017 at 15:58

    Hi Marc,

    please use the latest FW 3.5. If problem is still there, we'll find a way to solve It. Unfortunatelly I have not that device to reproduce the issue. 

    Thanks

    j

    Gerardo GALLUCCI
    ST Employee
    January 12, 2017
    Posted on January 12, 2017 at 19:20

    Hi Marc,

    Jan 29th 2016 was FW3.5 ->

    160129-c5bf5ce-SPWF01S

    Apr 10th 2015 was FW3.4 -> 

    150410-c2e37a3-SPWF01S

    Let me know if I can consider closed this issue.

    Thanks to you!

    jerry

    marc Georgin
    Associate
    January 13, 2017
    Posted on January 13, 2017 at 08:37

    Thanks ! This issue can be closed

    Gerardo GALLUCCI
    ST Employee
    January 13, 2017
    Posted on January 13, 2017 at 11:18

    Please use 'Mark Correct' button

    marc Georgin
    Associate
    February 8, 2017
    Posted on February 08, 2017 at 14:30

    Hello, 

    I have solved my problem with my P9 lite phone with the newer firmware version of the module. But with an other smartphone (Nexus 5X android 7) I can' connect to the AP of the module. When I click on the SSID in the WIFI parameter, the smartphone connects to the AP for few seconds then deconnects then reconnects for a few seconds .... and so on. I am working with a module with firmware 3.5 (the last).

    thanks for your help.

    Marc

    Gerardo GALLUCCI
    ST Employee
    February 8, 2017
    Posted on February 08, 2017 at 18:26

    Hi Marc,

    I suspect this is something added to miniAP after v3.5 (traffic information map bytes inside beacons). I can give you an updated FW, for a test. Send me a private message...

    marc Georgin
    Associate
    February 10, 2017
    Posted on February 10, 2017 at 12:43

    hello,

    have you received my message with my Email address ?

    regards.

    Marc

    Gerardo GALLUCCI
    ST Employee
    February 10, 2017
    Posted on February 10, 2017 at 14:36

    yes

    RobertoF
    Associate
    October 13, 2017
    Posted on October 13, 2017 at 09:22

    Hi Gerardo,

    I have a similar problem with HUAWEI P8 Lite (2015).

    It connects and disconnects continuously in a loop.

    Can You help me?

    I download and installed the app WIFI FIXER from Play store and I monitorized the thing.

    You can find the logs of the SPWF01 and of the app below. the firmware is 3.5 and the O.S. of the smartphone in Android 6.0.

    Best regards.

    This is the log from the of the SPWF01:

    +WIND:72:Station 5C:03:39:54:92:CC Disassociated:2

    +WIND:28:Station 5C:03:39:54:92:CC Associated:0

    +WIND:29:DHCP reply for 172.25.103.2/5C:03:39:54:92:CC

    +WIND:72:Station 5C:03:39:54:92:CC Disassociated:2

    +WIND:28:Station 5C:03:39:54:92:CC Associated:0

    +WIND:29:DHCP reply for 172.25.103.2/5C:03:39:54:92:CC

    +WIND:72:Station 5C:03:39:54:92:CC Disassociated:2

    +WIND:28:Station 5C:03:39:54:92:CC Associated:0

    +WIND:29:DHCP reply for 172.25.103.2/5C:03:39:54:92:CC

    +WIND:72:Station 5C:03:39:54:92:CC Disassociated:2

    +WIND:28:Station 5C:03:39:54:92:CC Associated:0

    +WIND:29:DHCP reply for 172.25.103.2/5C:03:39:54:92:CC

    +WIND:72:Station 5C:03:39:54:92:CC Disassociated:2

    +WIND:28:Station 5C:03:39:54:92:CC Associated:0

    And this is the log of the APP:

    Build:1.0.5:1165

    ALE-L21

    6.0

    2017-10-10 10:05:16: Network Check:

    2017-10-10 10:05:20: Network check failed: Trying again

    2017-10-10 10:05:20: I/O Exception172.25.103.1:HTTP_FAIL:4007ms

    2017-10-10 10:05:20: Current dBm:-56

    2017-10-10 10:05:20: WFMonitor Acquiring Wake Lock

    2017-10-10 10:05:20: Running Wifi Repair

    2017-10-10 10:05:20: Reassociating

    2017-10-10 10:05:20: WFMonitor Releasing Wake Lock

    2017-10-10 10:05:20: Fix Algorithm1

    2017-10-10 10:05:20: Supplicant State:ASSOCIATING

    2017-10-10 10:05:20: Supplicant State:ASSOCIATED

    2017-10-10 10:05:20: 'WIFI_TEC' : Network Disconnected

    2017-10-10 10:05:20: Supplicant State:COMPLETED

    2017-10-10 10:05:21: 172.25.103.1:HTTP_OK:1003ms

    2017-10-10 10:05:21: Current dBm:-56

    2017-10-10 10:05:21: WFMonitor Acquiring Wake Lock

    2017-10-10 10:05:21: Network Check:

    2017-10-10 10:05:21: 172.25.103.1:HTTP_OK:8ms

    2017-10-10 10:05:22: Current dBm:-56

    2017-10-10 10:05:22: WFMonitor Releasing Wake Lock

    2017-10-10 10:05:28: Demoting network'WIFI_TEC' to 61

    2017-10-10 10:05:36: Network Check:

    2017-10-10 10:05:36: 172.25.103.1:HTTP_OK:40ms

    2017-10-10 10:05:36: Current dBm:-56

    2017-10-10 10:05:36: Alarm Intent

    2017-10-10 10:05:56: Network Check:

    2017-10-10 10:05:56: 172.25.103.1:HTTP_OK:8ms

    2017-10-10 10:05:56: Current dBm:-56

    2017-10-10 10:06:16: Network Check:

    2017-10-10 10:06:16: 172.25.103.1:HTTP_OK:41ms

    2017-10-10 10:06:16: Current dBm:-57

    2017-10-10 10:06:36: Network Check:

    2017-10-10 10:06:36: 172.25.103.1:HTTP_OK:39ms

    2017-10-10 10:06:36: Current dBm:-56

    2017-10-10 10:06:56: Network Check:

    2017-10-10 10:06:56: 172.25.103.1:HTTP_OK:7ms

    2017-10-10 10:06:56: Current dBm:-56

    2017-10-10 10:07:16: Network Check:

    2017-10-10 10:07:20: Network check failed: Trying again

    2017-10-10 10:07:20: I/O Exception172.25.103.1:HTTP_FAIL:4007ms

    2017-10-10 10:07:20: Current dBm:-56

    2017-10-10 10:07:20: WFMonitor Acquiring Wake Lock

    2017-10-10 10:07:20: Running Wifi Repair

    2017-10-10 10:07:20: Reassociating

    2017-10-10 10:07:20: WFMonitor Releasing Wake Lock

    2017-10-10 10:07:20: Fix Algorithm1

    2017-10-10 10:07:20: Supplicant State:ASSOCIATING

    2017-10-10 10:07:20: Supplicant State:ASSOCIATED

    2017-10-10 10:07:21: 'WIFI_TEC' : Network Disconnected

    2017-10-10 10:07:21: Supplicant State:COMPLETED

    2017-10-10 10:07:21: 172.25.103.1:HTTP_OK:1004ms
    Gerardo GALLUCCI
    ST Employee
    October 29, 2017
    Posted on October 29, 2017 at 13:04

    Please test the FW3.5.3 (latest, online), and use the wifi_add_tim_ie/wifi_dtim_period variables (0/1 to dis/enable traffic information map information element).

    If also this release is not working, I assume it's something related to powersave of P8. SPWF01 miniAP  is not currently supporting powersaving STAs.

    RobertoF
    Associate
    October 30, 2017
    Posted on October 30, 2017 at 10:42

    Thank You very much but I've just tested the 3.5.3 changing the variables above, but without results.

    The distributor sent me a beta versione of firmware: SPWF01S-170213-7f49131-RELEASE-main and it works very well with P8 Lite but I'm waiting for the official release of it (I've some dubts with samsung galaxy S7). What's the differences between the two.

    Thank You in advance

    Gerardo GALLUCCI
    ST Employee
    October 30, 2017
    Posted on October 30, 2017 at 11:21

    You got a beta version of next release, allowing the module in miniAP to support powersaving STAs. Stay tuned.

    RobertoF
    Associate
    October 30, 2017
    Posted on October 30, 2017 at 11:50

    I'll be waiting for next release. I hope as soon as possible please.

    Thank you very much.