Skip to main content
Electronic1
Associate III
Jul 1, 2018 2:21 PM UTC
Question

SPBTLE-1S pinout configuration

Posted on July 01, 2018 at 16:21

Hello, 

I am trying to develop a new product with the SPBTLE-1S module, my idea is to use the module connected to a uC by UART.

https://www.st.com/resource/en/datasheet/spbtle-1s.pdf

 

Looking in the datasheet I see that the pinout description changes depending on the 'Mode', but I can't find anywhere how these modes are set.

Could anyone help me?

I am on the point of defining the hardware connections.

Many thanks

#spbtle-1s
    This topic has been closed for replies.

    2 replies

    Winfred LU
    ST Employee
    Jul 2, 2018 5:38 AM UTC
    Posted on July 02, 2018 at 07:38

    Hi Bernat,

    SPBTLE-1S is a module based on BlueNRG-1 SoC.

    Please refer to  

    https://www.st.com/resource/en/datasheet/bluenrg-1.pdf

     , Section 3.12

    Best Regards,

    Winfred

    Michael Krechko
    Associate
    Jul 7, 2018 6:37 AM UTC
    Posted on July 07, 2018 at 08:37

    Try to use 'Chat' example from SDK, it provides UART<->BLE or 'DTM' example if you want to have direct HCI access to BLE stack