Skip to main content
Chithambara Ganesh
Associate
January 25, 2017
Solved

I am not able to get exact information for footprint creation of LSM9DS1, can anyone help pls

  • January 25, 2017
  • 3 replies
  • 1028 views
Posted on January 25, 2017 at 05:13

0690X00000603ZwQAI.jpg

x = ?

y= ?

z = ?

    This topic has been closed for replies.
    Best answer by Miroslav BATEK
    Posted on January 25, 2017 at 10:49

    All the pads are the same.

    x = M = typ. 0.1 mm

    y = T1 = typ. 0.35mm

    z = E1 - T1 - 2xM = typ. 2.95mm

    3 replies

    Miroslav BATEKBest answer
    ST Employee
    January 25, 2017
    Posted on January 25, 2017 at 10:49

    All the pads are the same.

    x = M = typ. 0.1 mm

    y = T1 = typ. 0.35mm

    z = E1 - T1 - 2xM = typ. 2.95mm

    Chithambara Ganesh
    Associate
    January 25, 2017
    Posted on January 25, 2017 at 11:49

    Thanks Miroslav for your reply,

    from your reply i am understanding in following way, Please correct me if i am wrong,

    1) x = distance between component right edge and right edge of pin5

    it is same as 'distance between component bottom edge &  bottom edge of pin 13' which is M=0.1mm

    2) y = Pad width of pin 17

    All pads from 1-18 are of same size

    So y=T1=0.35mm

    3) z= distance between center of Pins  2 and 17

    z=E1-T1(pad width of pin 17)-2xM

    so Z=2.95mm

    Please conform ASAP.

    ST Employee
    January 25, 2017
    Posted on January 25, 2017 at 12:08

    Yes, your understanding is correct.