Skip to main content
Nicolino Piergiovanni
Visitor II
April 23, 2018
Question

mbedtls server error on firefox

  • April 23, 2018
  • 0 replies
  • 676 views
Posted on April 23, 2018 at 09:54

Hi all.

I would like to use a SSL connection, so I tried  the mbedtls server example found in

STM32Cube_FW_F7_V1.9.0\Projects\STM32F769I-Discovery\Applications\mbedTLS\SSL_Server

I used IAR_760 with no code optimization and Firefox 56.0 32bit as browser.

The discovery is connected directly to my PC, no DHCP, and fixed address 192.168.1.10 is set.

Before to start with SSL session I sent a ping to discovery to check the ethernet link. All OK.

When I start with the SSL connection

https://192.168.1.10:4433

the answers on discovery display are:

Waiting for a remote connection...... OK

Performing the SSL/TLS handshake ..... failed

mbedtls_ssl_handshake returned -19056 (MBEDTLS_ERR_SSL_INVALID_MAC)

Walking in the code I found the problem around these functions:

File ssl_tls.c

1567         static int ssl_decrypt_buf( mbedtls_ssl_context *ssl )

                  .

                  .

                  .

        /*

         * Decrypt and authenticate

         */

        if( ( ret = mbedtls_cipher_auth_decrypt( &ssl->transform_in->cipher_ctx_dec,

                                         ssl->transform_in->iv_dec,

                                         ssl->transform_in->ivlen,

                                         add_data, 13,

                                         dec_msg, dec_msglen,

                                         dec_msg_result, &olen,

                                         dec_msg + dec_msglen, taglen ) ) != 0 )

        {

            MBEDTLS_SSL_DEBUG_RET( 1, 'mbedtls_cipher_auth_decrypt', ret );

1678            if( ret == MBEDTLS_ERR_CIPHER_AUTH_FAILED )  <------------------------

                return( MBEDTLS_ERR_SSL_INVALID_MAC );

            return( ret );

        }

Any suggestions?

Thank in advance

    This topic has been closed for replies.