Skip to main content
Parmin Nayani
Associate III
March 20, 2017
Question

STM32l151RBT6A SPI issue

  • March 20, 2017
  • 5 replies
  • 1080 views
Posted on March 20, 2017 at 13:57

Hi all,

I am not able to get SPI working on stm32l151rbt6a. I have posted my initialization code below.

/* SPI1 init function */

void MX_SPI1_Init(void)

{

     GPIO_InitTypeDef GPIO_InitStruct;

     SPI_HandleTypeDef hspi1;

        __SPI1_CLK_ENABLE();            // clock ok

        /**SPI1 GPIO Configuration

        PA5     ------> SPI1_SCK

        PA6     ------> SPI1_MISO

        PA7     ------> SPI1_MOSI

        */

        GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;

        GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

        GPIO_InitStruct.Pull = GPIO_NOPULL;

        GPIO_InitStruct.Speed = GPIO_SPEED_VERY_LOW;

        GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;

        HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  hspi1.Instance = SPI1;

  hspi1.Init.Mode = SPI_MODE_MASTER;

  hspi1.Init.Direction = SPI_DIRECTION_2LINES;

  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;

  hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;

  hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;

  hspi1.Init.NSS = SPI_NSS_SOFT;

  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;

  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;

  hspi1.Init.TIMode = SPI_TIMODE_DISABLED;

  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLED;

  HAL_SPI_Init(&hspi1);

  __HAL_SPI_ENABLE(&hspi1);

 }

I am writing a byte to DR and  waiting for RXNE bit to set. RXNE bit is never setting. What could be the problem? I have spent a lot of time trying various options but to no avail. Any help will be highly appreciated. Thank you in advance.

    This topic has been closed for replies.

    5 replies

    Khouloud GARSI
    ST Employee
    March 21, 2017
    Posted on March 21, 2017 at 15:38

    Hi

    Nayani.Parmin

    ‌,

    I'd highly recommend you to refer to the SPI examples under

    http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubel1.html

    package.

    The 'SPI' examples are found under the path below:

    STM32Cube_FW_L1_V1.6.0\Projects\STM32L152RE-Nucleo\Examples\SPI

    Those examples runs on STM32L1xx devices; They will help you to correctly configure the SPI peripheral.

    Khouloud.

    Parmin Nayani
    Associate III
    March 22, 2017
    Posted on March 22, 2017 at 04:16

    Hi Khouloud,

    As a matter of fact I used the code generated by Cube only. However I will go through the link, check and revert. If you have worked on this controller SPI, did you get it working? Thank you.

    Khouloud GARSI
    ST Employee
    March 22, 2017
    Posted on March 22, 2017 at 12:04

    Hi

    Nayani.Parmin

    ‌,

    The examples are working conveniently.

    Khouloud.