Skip to main content
Luca DC
Associate II
Sep 5, 2017 8:47 AM UTC
Question

Connecting SPWF01SA to hidden SSID

Posted on September 05, 2017 at 10:47

Hi,

I need to have a SPWF01SA module connect to a Wi-Fi router with hidden SSID.

The first operation the module tries upon starting is '+WIND:21:WiFi Scanning' which completes with the result '+WIND:35:WiFi Scan Complete (0x0)' so the handshake can't proceed.

The module is already fully configured with SSID, password, DNS and so on. It connects successfully as soon as the SSID is made visible.

How can I overcome the void scanning at the beginning and force the connection?

Thank you for your help.

#spwf01sa
    This topic has been closed for replies.

    5 replies

    Gerardo GALLUCCI
    ST Employee
    Oct 29, 2017 12:37 PM UTC
    Posted on October 29, 2017 at 13:37

    Use latest FW 3.5.3.

    Then, use wifi_region (default: 1; set >= 2) variable to allow module to perform an active scan, and find hidden AP.

    By default, module will not perform an active scan into channels where there is no activity.

    Varadharajan V
    Associate III
    Dec 21, 2017 10:29 AM UTC
    Posted on December 21, 2017 at 10:29

    Even with the latest firmware, module not connects with hidden AP