Associate
February 28, 2017
Question
unable to flash the development SPC560B-Dis
- February 28, 2017
- 6 replies
- 1503 views
Posted on February 28, 2017 at 11:42
#development-board #spc5-studio #spc560b-dis
Hi All,
Appreciate your time and help.
i am using the SPC560B-DIS development board with the spc5studio IDE.
all of a sudden when i tried to flash the development board i got an error in the log saying : Error, Core::PpcJtagTargIntf, Connection to target lost !
i suspected a loose cable to be the culprit but then the same cable works perfectly fine with the other EVM(evaluation board).Then i also checked the mini usb power/debug female port connector on the board which is fine as well.(did not see any physical damage on it attached is the image below).i have attached my boards log file from the UDE when i got the board connection lost error.
#development-board #spc5-studio #spc560b-dis