Skip to main content
Santhamurthy R
Associate III
March 10, 2017
Solved

Unable to generate Source for EED

  • March 10, 2017
  • 5 replies
  • 1514 views
Posted on March 10, 2017 at 14:55

Hello All,

I am using SPC560B540L5 Discovery board and SPC stdutio 5.2.3 updated version code generator.

I am trying to emulate the Flash as EEPROM using EED driver. The IDE is installed with EEPROM emulation software and the way I generate the project is also proper even then the necessary configuration files and libraries for EED are not getting generated after generating the code. Normally, it should get listed under the EEPROM Emulation driver in components directory, but nothing exists other than ''mak'' folder. Please find the snap below.

0690X000006067SQAQ.png

But still I tried to build the project but the compilation failed due to below shown error.

0690X00000606YDQAY.png

I also tried with the Test application''SPC560Bxx_RLA EE Test Application for Discovery'' but the problem repeats.

Even I tried with different versions of (SPC5studio) 5.0.0, 5.2.1 and 5.2.3 but nothings works.

Kindly help in getting the problem resolved.

Thanks in Advance

Regards,

R.Santhamurthy

    This topic has been closed for replies.
    Best answer by Erwan YVIN
    Posted on March 13, 2017 at 11:22

    Hello R. SanthaMurphty ,

    The problem has been reproduced on 5.2.3

    it will be solvedofficially on 5.3.0.

    Anyway, you can install these new eeprom feature by local update

    (Uncheck Category)

    it solves the issue

    Best regards

    Erwan

    ________________

    Attachments :

    com.st.spc5.components.ee.spc56xx.feature.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyoG&d=%2Fa%2F0X0000000bCf%2Fq6FIo_IjnNRyxdR6tPnKjR0P_iipVTeUOHLhDbGJr0k&asPdf=false

    5 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    March 13, 2017
    Posted on March 13, 2017 at 11:22

    Hello R. SanthaMurphty ,

    The problem has been reproduced on 5.2.3

    it will be solvedofficially on 5.3.0.

    Anyway, you can install these new eeprom feature by local update

    (Uncheck Category)

    it solves the issue

    Best regards

    Erwan

    ________________

    Attachments :

    com.st.spc5.components.ee.spc56xx.feature.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyoG&d=%2Fa%2F0X0000000bCf%2Fq6FIo_IjnNRyxdR6tPnKjR0P_iipVTeUOHLhDbGJr0k&asPdf=false
    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Santhamurthy R
    Associate III
    March 13, 2017
    Posted on March 13, 2017 at 12:26

    Hi Erwan,

    I uninstalled and reinstalled EEPROM Emulation software from the Eclipse Marketplace and regenerated the code after restarting the IDE, but the problem didn't resolved.

    What do mean by local update,Kindly suggest some quick solution or at least  share the necessary source libraries related to EED since it is blocking issue for my development.

    Kindly do the needful.

    0690X00000606JjQAI.png

    Thanks in Advance,

    Regards,

    R.Santhamurthy

    Santhamurthy R
    Associate III
    March 30, 2017
    Posted on March 30, 2017 at 15:43

    Hi Erwan,

    Thanks for providing the source for EED component.

    While working only with EED component the application is working fine. But when I am trying to add both Flash and EED component together in the application, it is giving error as 'conflicting types for FlashInit()', since the prototype for the FlashInit() differs in eed_flash.h of EED component and ssd_c90fl.h of Flash component.

    In my application I should use both the EED and Flash components.i am attaching my test application with this kindly check and provide your valuable suggestion for resolving the reported issue.

    ________________

    Attachments :

    Bootloader.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hyfe&d=%2Fa%2F0X0000000bBs%2FBPxgSvRx0MUI520Hx66F3RVgQ45ZpYIrOwrTXUtpEzQ&asPdf=false