Question
STM32F4XX HAL ETH initial LAN8720A bug
Posted on August 08, 2017 at 09:43
My hardware is F429 + LAN8720A, firmware is STM32Cube_FW_F4_V1.16.0
when power up, everything is ok, PHY_BCR = 0x3100, phy link up, at this time I just reset f429,
PHY_B
C
R = 0x2100, PHY link failed, and the two leds are off.Here are some codes in the HAL driver:

My question is after reset we should set the BCR, but the HAL driver reset the BCR, then just wait link up, is that right?