4 Bytes repeating when using memcpy
Hi ,
We are using Cortex-M4(STM32F429IIH6) processor for our IOT project. We are seeing a data corruption when memcpy used, the corruption pattern was identified by feeding a Fixed pattern of size 512 Bytes from Src to Dest using memcpy, and it is not happening in all the iterations.
If you see the image attached below that Data '6 N 7 O' is replaced with 2 Bytes('Highlighted with orange color' 4L).
Can any one tells that what can be the reason for this wired behavior? We are in a critical phase of our project.
Regards,
Krishna Prasad