STM32L433: Using PH0 PH1 as GPIO
Hi,
I realized a prototype including the STM32L433 (LQFP64 package). I tried to use the pins PH0 and PH1 as OUTPUT pins. This should be possible according to the datasheet (5V tolerant I/O pins). This pins can be used to attach a crystal or oscillator to the controller. This external clock would act as
HSE
, which I do not use (haven't installed). So disabled the HSE as well as the LSE.I wasn't able to set the pins PH0 and PH1 HIGH. Interestingly, for the pins PC14 and PC15, which are responsible for the
LSE
, it works fine. I defined the pins PH0, PH1, PC14 and PC15 in as push-pull outputs.Is it possible to use PH0 & PH1 as GPIO pins, or have I missed something in the datasheet?
BR
#hse #stm32l433 #gpio #push-pull #output