Skip to main content
Simon NOWAK
Associate II
March 9, 2017
Question

ADC dynamic range : How can I the maximum ADC conversion precision ?

  • March 9, 2017
  • 3 replies
  • 1301 views
Posted on March 09, 2017 at 09:27

Hi everyone,

I work with the stm32l073rz. I  measure the sensor with the ADC and the retrieved value is correct.

Now, I want to increase the precision. The sensor gives a little value (maximum 1.5V). Can I reduce the intern ADC voltage to increase the precision like this figure ?

Thank you very much for your help

Regards

Simon

0690X00000606WMQAY.png

#nucleo: #adc #vref+ #stm32l0
This topic has been closed for replies.

3 replies

S.Ma
Principal
March 9, 2017
Posted on March 09, 2017 at 09:52

Assuming calibration is done, using oversampling (if possible) would be the first step to less noise.

The VDDA should be a clean non noisy source (PSSR power rejection impacting the precision and performance).

In theory, reducing VDDA might help 'less than' a bit. Your main goal is to reduce the SNR.

If the signal is not random and is characterized, digital filtering post processing may also help.

Simon NOWAK
Associate II
March 10, 2017
Posted on March 10, 2017 at 10:26

Hi,

Thanks for your answer, you helped me.

Now, I write in the CFGR2 register to modify the oversampling ratio but I have a problem to re-activate the CKMODE bits. 

I can't never write in

the CKMODE bits, I can just reset this bits. 

Regard,

Simon

AvaTar
Senior III
March 10, 2017
Posted on March 10, 2017 at 10:42

Wouldn't adding a buffer amplifier (x 2.2 = 3.3V / 1.5V) do the same job ?

It would relax possible input impedance issues as well.