Skip to main content
Matthew Lai
Associate II
March 8, 2017
Solved

DCMI + FMC on STM32F7

  • March 8, 2017
  • 2 replies
  • 842 views
Posted on March 08, 2017 at 17:57

Hello!

From a cursory glance at the datasheet it seems like there are many pin conflicts between DCMI and FMC on the F7. Does that mean they cannot be used at the same time?

Isn't that a bit of an oversight, considering image data often take quite a bit of memory?

Thanks

Matthew

    This topic has been closed for replies.
    Best answer by Tesla DeLorean
    Posted on March 08, 2017 at 18:05

    Perhaps, it depends on how many pins your chosen device has, and the may be overlap or alternate options. Historically some of the AF muxing choices had been a bit brain damaged. (SDIO or ETHERNET vs LCD on the STM32F429I-DISCO)

    Haven't done the due diligence on the pins here, does CubeMX provide escape on the maximal pin product?

    2 replies

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    March 8, 2017
    Posted on March 08, 2017 at 18:05

    Perhaps, it depends on how many pins your chosen device has, and the may be overlap or alternate options. Historically some of the AF muxing choices had been a bit brain damaged. (SDIO or ETHERNET vs LCD on the STM32F429I-DISCO)

    Haven't done the due diligence on the pins here, does CubeMX provide escape on the maximal pin product?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Matthew Lai
    Associate II
    March 8, 2017
    Posted on March 08, 2017 at 18:25

    Ahh yes of course. Had a brain fart, thanks!

    Forgot they can be on multiple pins!