ADC with DMA with SW Trigger on L486 MCU
- June 9, 2017
- 5 replies
- 2251 views
I wish to use ADC1 to measure 6 channels and to have the results DMAd into memory.
I am using CubeMX V4.21 and I think that I have set the parameters up correctly
(See attached screen snip ADC_DMA_1 to 3.PNG)
This sequence is to be triggered by S/W to run once, terminate and then run again sometime later.
(This is in a loop for testing at the moment).
The DMA happens as I am seeing the ADC readings appear in the adc1_data array and I get the DMA half complete interrupt handler being called but not the end of sequence interrupt.
What am I doing wrong please.....
My code is :-
uint16_t adc1_data[6];#define ADC1_BUFFER_SIZE_IN_BYTES 12
#define ADC1_TEMP1_OFFSET 0
#define
ADC1_TEMP2_OFFSET 1#define
ADC1_VBOOST_OFFSET 2#define
ADC1_VHLC_OFFSET 3#define
ADC1_INTERNAL_TEMP_OFFSET 4#define
ADC1_VREF_OFFSET 5volatile bool adc1_active_flag;
void start_adc1(void){ HAL_StatusTypeDef status;set_VDDA_PWR_EN(ANALOG_POWER_ON);
set_nVMON_ENABLE(VMON_ENABLE_ON); set_nTEMP_SENSOR_PWR_EN(TEMP_SENSOR_POWER_ON);adc1_active_flag = TRUE;
osDelay(2);
status = HAL_ADCEx_Calibration_Start(&hadc1, ADC_SINGLE_ENDED);
if(HAL_OK != status) { // Blah }status = HAL_ADC_Start_DMA(&hadc1, (uint32_t *)adc1_data, ADC1_BUFFER_SIZE_IN_BYTES);
if(HAL_OK != status) { // Blah }}void HAL_ADC_ConvHalfCpltCallback(ADC_HandleTypeDef* hadc)
{ static bool apapap; if(ADC1 == hadc->Instance) { // Voltage subsystem... apapap = TRUE; // <<< Gets here.... } if(ADC2 == hadc->Instance) { // Blah }if(ADC3 == hadc->Instance)
{ // Blah }}void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc){ if(ADC1 == hadc->Instance) { if(__HAL_ADC_GET_FLAG(hadc, ADC_FLAG_EOS)) // << Never gets here...:(
{ // Voltage subsystem... adc1_active_flag = FALSE; set_nTEMP_SENSOR_PWR_EN(TEMP_SENSOR_POWER_OFF); set_nVMON_ENABLE(VMON_ENABLE_OFF); } if(__HAL_ADC_GET_FLAG(hadc, ADC_FLAG_EOC)) { // Voltage subsystem... adc1_active_flag = FALSE; set_nTEMP_SENSOR_PWR_EN(TEMP_SENSOR_POWER_OFF); set_nVMON_ENABLE(VMON_ENABLE_OFF); } } if(ADC2 == hadc->Instance) { // Blah } if(ADC3 == hadc->Instance) { // Blah }} // freeRTOS task... // /* Infinite loop */ for(;;) { if(MODE_BLAH == my_mode) { osDelay(1000);// We have been woken so do something...
start_adc1();// Block until the scan has completed...
// Better way would be to use a mutex block here... [AP] while(TRUE == read_adc1_active_flag()) { ; }len = sprintf(adc1_test, 'T1:%d\tT2%dVB:%d\tVHLC:%d\tMCU_Temp:%d\tVref:%d\n',
adc1_data[ADC1_TEMP1_OFFSET], adc1_data[ADC1_TEMP2_OFFSET], adc1_data[ADC1_VBOOST_OFFSET], adc1_data[ADC1_VHLC_OFFSET], adc1_data[ADC1_INTERNAL_TEMP_OFFSET], adc1_data[ADC1_VREF_OFFSET]);// Trace the output...
str_trace('ADC Vals:%s', adc1_test);}
}