Skip to main content
Aaron Derbyshire
Associate III
November 30, 2017
Solved

LIS3DH: 12 Bit Resolution and FIFO Mode

  • November 30, 2017
  • 4 replies
  • 1852 views
Posted on November 30, 2017 at 11:19

Given that the LIS3DH FIFO is only 10 bit wide, is it actually possible to run the accelerometer with 12 bit resolution?

#12-bit #lis3dh #fifo
This topic has been closed for replies.
Best answer by Miroslav BATEK
Posted on December 01, 2017 at 17:40

I think if the sensor is configured int Low-power mode (8-bit resolution) also only 8-bit value is stored in the FIFO (the low bytes are 0).

4 replies

ST Employee
November 30, 2017
Posted on November 30, 2017 at 16:09

If FIFO is disabled and the sensor is configured into High-resolution mode the output is 12-bit.

0690X0000060925QAA.png
Aaron Derbyshire
Associate III
November 30, 2017
Posted on November 30, 2017 at 16:21

As I anticipated, thank you.

Does this mean that similarly if I have the sensor configured into a FIFO mode with 8 bit resolution I will still achieve 8 bit resolution?

Miroslav BATEKBest answer
ST Employee
December 1, 2017
Posted on December 01, 2017 at 17:40

I think if the sensor is configured int Low-power mode (8-bit resolution) also only 8-bit value is stored in the FIFO (the low bytes are 0).