Question
Wav player using DAC in STM32F429
Posted on July 26, 2017 at 13:32
Hello,
I noticed that the stm32F429 disco does not have the CS43L22 circuit nor a 3.5mm jack for audio output as its rival the F407, but it has two internal DAC output, which can be used to play a wav file.
If anyone has an example compatible with HAL libraries would be very nice !
Farouk
#stm32f429-disco #wav