Skip to main content
Paul Sidorov
Associate
August 21, 2017
Question

HAL and STD libraries

  • August 21, 2017
  • 4 replies
  • 2160 views
Posted on August 21, 2017 at 13:23

Hi!! Project(STM32F4) is written using the STD library, but in HAL libary much easier to work with ethernet. How do you think it is possible  to use HAL and STD library together?  

#stm32f4 #std_lib #hal
This topic has been closed for replies.

4 replies

Szymon PANECKI
Senior III
August 21, 2017
Posted on August 21, 2017 at 14:23

Hello Paul,

In order to have a consistent project it would be much better to use one approach. Maybe you can consider porting Standard Peripheral Library code to HAL code. Recently we introduced a tool, which makes such conversion automatically. It is called

http://www.st.com/en/development-tools/spl2ll-converter.html

. This tool converts SPL code to HAL LL code (because SPL is much more similar to HAL LL comparing to standard HAL).

Regards

Szymon

Tuttle.Darrell
Associate II
August 21, 2017
Posted on August 21, 2017 at 14:48

Hello Szymon,

I too am possibly interested in the converter; but just as the OP has specified STM32F4, we have a large SPL code base used with STM32F4. From the page you linked to:

It ensures full migration within a given STM32 series and partial migration across STM32 series. The migration is possible only for STM32 peripherals covered by STM32Cube LL drivers.

I have asked in other threads how much is STM32F4 supported in LL drivers (or will be), as it doesn't appear like there is much. My question has never been answered by ST. Is there a document that details what support there will be in terms of LL for STM32F4? This is the primary reason we have resisted making the move to STM32CubeMX and HAL.

Thanks,

Darrell

Szymon PANECKI
Senior III
August 21, 2017
Posted on August 21, 2017 at 18:21

Hello Darrell,

I have just checked the STM32F4Cube package, latest revision (1.16). HAL LL supports these peripherals:

ADC, CRC, DAC, DMA, DMA2D, EXTI, FMC, FSMC, GPIO, I2C, LPTIM, PWR, RCC, RNG, RTC, SDMMC, SPI, TIM, USART, USB.

I agree that these are not all peipherals, which we can find across all MCUs in STM32F4 family, but at least most of the standard peripherals seems to be covered by LL.

Regarding your question concernign STM32F4 support  for LL - within two next months new release of CubeMX is expected - version 4.23. It will allow to generate code for STM32F4 based on HAL LL. Now this tool allows doing it for some STM32 families (like L0, F0, L4), but not yet for F4. So this feature will be added.

Regards

Szymon