Skip to main content
Matteo Pirro
Visitor II
March 22, 2017
Question

H3LIS331DL Configuration Doubts

  • March 22, 2017
  • 1 reply
  • 630 views
Posted on March 22, 2017 at 10:40

Hi,

I'm working with H3LIS331DL MEMS sensor. I read the IC datasheet many times, but I still have some doubts on how to configure it. In particular I ask you:

  • INT_THS register: it is a 7bit threshold while data is a 12bit value. This means the threshold resolution is lower? I have 2^7 level from 0 to Full Scale value? Am I right?
  • INT_DUR register: datasheet says duration step depends on ODR chosen. This means if I set a INT_DUR = 0x0A and ODR=1000 duration is 10ms, while if ODR is 10 (low power) duration is 1sec? Am I rigth?
  • INT_CFG register: ZHIE=1 means interrupt will fire when |acceleration| > Threshold while ZLIE=1 means interrupt will fire when |acceleration| < Threshold. Right?

Thank you for your support.

PS I suggest to insert this kind of information on the datasheet because in my opinion is not clear at all.

Matteo

#h3lis331dl-configuration
    This topic has been closed for replies.

    1 reply

    ST Employee
    September 29, 2017
    Posted on September 29, 2017 at 15:39

    You are right, your assumptions are absolutely correct.