Skip to main content
Jason Smith
Associate II
April 3, 2017
Solved

STM32F103 - Std Periph Driver not working with bootloader

  • April 3, 2017
  • 8 replies
  • 1792 views
Posted on April 03, 2017 at 05:58

I am running into an issue with the ST Standard Peripheral Driver. If I download my project to my STM32F103 at Vector 0x08000000, it runs fine. If I use my bootloader to load my project to 0x08004000 (I set this in the linker tab as well), it will not work. Other projects work fine when using the bootloader but this project is my first one with the Std. Periph. Driver. Does the driver expect vector 0x08000000 somewhere that I need to edit a source or header file?

    This topic has been closed for replies.
    Best answer by Jason Smith
    Posted on April 08, 2017 at 06:18

    Disregard. I figured it out.  I was using the Standard Peripheral Driver in my bootloader as well as my program.  I wasn't calling RCC_DeInit().  I added that right before I jump to location 0x8004000 in my bootloader and now my bootloaded program works.

    8 replies

    Tesla DeLorean
    Guru
    April 3, 2017
    Posted on April 03, 2017 at 06:26

    Make sure SCB->VTOR is set correctly in system_stm32f10x.c, see end of SystemInit(), and defines.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Jason Smith
    Associate II
    April 3, 2017
    Posted on April 03, 2017 at 13:36

    Does the periph driver use SCB->VTOR?  I don't have to set this in my other projects that bootload correctly.

    Tesla DeLorean
    Guru
    April 3, 2017
    Posted on April 03, 2017 at 15:39

    I've told you twice that it does. 

    http://www.keil.com/forum/62419/

     

    >>

    I don't have to set this in my other projects that bootload correctly.

    But presumably you want to fix the ones that aren't working, so focus on them.

    Make sure to enable interrupts if you disable them.

    Make sure you service interrupts you have enabled, or turn them off before the hand-over.

    SystemInit() will also tear down clocks and PLL settings, this frequently isn't required.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    April 3, 2017
    Posted on April 03, 2017 at 16:19

    STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Template\system_stm32f10x.c

    ...

    /*!< Uncomment the following line if you need to relocate your vector Table in

    Internal SRAM. */

    /* ♯ define VECT_TAB_SRAM */

    ♯ define VECT_TAB_OFFSET 0x0 /*!< Vector Table base offset field.

    This value must be a multiple of 0x200. */

    ...

    /**

    * @brief Setup the microcontroller system

    * Initialize the Embedded Flash Interface, the PLL and update the

    * SystemCoreClock variable.

    * @note This function should be used only after reset.

    * @param None

    * @retval None

    */

    void SystemInit (void)

    {

    ...

    ♯ ifdef VECT_TAB_SRAM

    SCB->VTOR = SRAM_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal SRAM. */

    ♯ else

    SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH. */

    ♯ endif

    }
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..