Question
STM32L4 USBD receive
Posted on September 22, 2017 at 15:45
I am currently using the 'STM32CubeFunctionPack_MOTENV1_V3.0.0' for SensorTile platform.
I does support the USBD_cdc function in sending data to PC (Print) but missing the receive code.
Since there is a ST BLE on board, I would like to connect with the 'BlueNRG GUI' tools which I can perform firmware update through USB for ST-BLE.
1. Where I could find the example code for USBD receive for STM32L4 ?
2. Is 'BlueNRG DK 2.0.2\Projects\Projects_Cube\BlueNRG_Stack_IFR_Updater' be the right package to start ?
Thanks