Skip to main content
Johannes Trepte
Associate
April 5, 2017
Question

STM32L431 COMP erratum

  • April 5, 2017
  • 2 replies
  • 869 views
Posted on April 05, 2017 at 12:04

On the STM32L431, there's an erratum described in STM32L431xx Errata sheet (STM32L431xx device limitations / DM00218224). It allows to reset COMP1 and COMP2 despite of the LOCK bit being set.

My question: What happens to an I/O pin that is connected to the COMP's output via the alternate function multiplexer / GPIOx_AFR? Will it switch to a defined state? If so, to which state?

#comp-erratum
    This topic has been closed for replies.

    2 replies

    Amel NASRI
    ST Technical Moderator
    April 5, 2017
    Posted on April 05, 2017 at 16:03

    Hello

    trepte.johannes

    ‌,

    Setting SYSCFGRST will restSYSCFG + COMP + VREFBUF, so it has no impact on GPIO registers even if the pin is configured in AF mode to be used as Comp output.

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
    Johannes Trepte
    Associate
    April 5, 2017
    Posted on April 05, 2017 at 16:37

    Hello Amel,

    thanks for your quick response.

    I understand that SYSCFGRST will not change GPIO registers.

    But what about the voltage at the pin itself? The GPIO pin remains configured as an alternate function, connected to the COMP peripheral, which itself will be reset. What information will the COMP output pass to the GPIO driver?

    • Always 0?
    • Always 1?
    • Unchanged?
    • Undefinded?

    This information would be important for me in order to implement a defined (save) state if the COMP gets reset.

    Johannes