Skip to main content
Patrick Morwald
Associate III
Mar 22, 2018 10:47 AM UTC
Question

JTAG connection to STM32F407 with ST-Link V2 is not working

Posted on March 22, 2018 at 11:47

I am trying to debug my STM32F407 based board with the ST-LinkV2 adapter. It works fine when i use SWD, but i cannot get a JTAG connection.

Here is the error i get when trying to connect via JTAG:

Wrong device detected

Open On-Chip Debugger 0.10.0-dev-00007-g58350bc-dirty (2018-01-08-12:20)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/html/bugs.html

srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter_nsrst_delay: 100

adapter speed: 1125 kHz

Info : tcl server disabled

Info : telnet server disabled

Info : clock speed 1125 kHz

Info : STLINK v2 JTAG v29 API v2 SWIM v7 VID 0x0483 PID 0x3748

Info : vid/pid are not identical: 0x0483/0x374B 0x0483/0x3748

Info : using stlink api v2

Info : Target voltage: 3.212598

Error: init mode failed (unable to connect to the target)

in procedure 'init'

in procedure 'ocd_bouncer'

I connected my ST-LinkV2 to the STM32F407VGTx (LQFP100) in the following way:

ST-Link P1 (VAPP) -> STM32 VDD

ST-Link P6 (GND) -> STM32 GND

ST-Link P5 (JTDO) -> STM32 PA15 (JTDI)

ST-Link P13 (JTDI) -> STM32 PB3 (JTDO)

ST-Link P7 (JTMS) -> STM32 PA13 (JTMS)

ST-Link P9 (JTCK) -> STM32 PA14 (JTCK)

But i cannot connect to my processor, neither with St-Link utility nor can i start a debug session with SW4STM32 IDE.

I use 1,25 MHz JTAG since i think thats the maximum the St-Link V2 supports?

Please help.

This topic has been closed for replies.

4 replies

Patrick Morwald
Associate III
Mar 29, 2018 1:57 PM UTC
Posted on March 29, 2018 at 15:57

Bump. This is an important question for us.

Andrew Neil
Super User
Mar 29, 2018 3:58 PM UTC
Posted on March 29, 2018 at 17:58

Can you connect using the 

http://www.st.com/en/development-tools/stsw-link004.html

  ?

You should try with this first - to see it it's a fundamental issue, or just a problem with the 

SW4STM32 IDE ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Patrick Morwald
Associate III
Mar 29, 2018 4:11 PM UTC
Posted on March 29, 2018 at 18:11

Hi,

thanks for the answer but i tried already.

Bruno Conceição
Associate II
Jan 24, 2019 5:41 PM UTC

Hi Patrick,

did you found what the problem was? I'm facing the same issue...

Thanks,