Question
Controlling a sensorless 15W BLDC motor using STEVAL-SPIN3202
Posted on January 18, 2018 at 23:26
I'm using a STEVAL-SPIN3202 to control a 15W BLDC sensorless motor. I'm unable to spin a motor using six-step driving mode and I'm assuming it's because the motor's configuration needs to be updated. Looking at the #defined MC_SixStep_param_32F0.h configuration file the only motor parameter that I can find is the number of pole pairs. Is there an additional configuration file for the motor? Any help would be greatly appreciated!