Issue in readings of internal Temperature Sensor
Hi Guys,
am using STM32f429, trying to read internal temperature sensor which is configured to ADC1 ADC_CHANNEL_18,
am able to read temperature readings,but my device is giving 70 deg/C .
am not able to find why the device is giving temperature that much high, following is the code which am using,
#define ADC_CHANNEL_DIFFERENCIATION_TEMPSENSOR_VBAT 0x10000000U
#define ADC_CHANNEL_TEMPSENSOR ((uint32_t)ADC_CHANNEL_18 |ADC_CHANNEL_DIFFERENCIATION_TEMPSENSOR_VBAT)
#define ADC_CHANNEL_VREFINT ((uint32_t)ADC_CHANNEL_17)#define ADC_CHANNEL_VBAT ((uint32_t)ADC_CHANNEL_18)void TempINIT(void){
ADC_ChannelConfTypeDef sConfig;
AdcHandle.Instance = ADC1; AdcHandle.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV2; AdcHandle.Init.Resolution = ADC_RESOLUTION12b; AdcHandle.Init.ScanConvMode = DISABLE; /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */ AdcHandle.Init.ContinuousConvMode = DISABLE; /* Continuous mode disabled to have only 1 conversion at each conversion trig */ AdcHandle.Init.DiscontinuousConvMode = DISABLE; /* Parameter discarded because sequencer is disabled */ //AdcHandle.Init.NbrOfDiscConversion = 0; AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; /* Conversion start trigged at each external event */ AdcHandle.Init.ExternalTrigConv = ADC_SOFTWARE_START;//ADC_EXTERNALTRIGCONV_T1_CC1; AdcHandle.Init.DataAlign = ADC_DATAALIGN_RIGHT; AdcHandle.Init.NbrOfConversion = 1; AdcHandle.Init.DMAContinuousRequests = DISABLE; AdcHandle.Init.EOCSelection = ADC_EOC_SINGLE_CONV;if (HAL_ADC_Init(&AdcHandle) != HAL_OK)
{ /* ADC initialization Error */ Error_Handler(); }/*##-2- Configure ADC regular channel ######################################*/
sConfig.Channel = ADC_CHANNEL_TEMPSENSOR ; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;if (HAL_ADC_ConfigChannel(&AdcHandle, &sConfig) != HAL_OK)
{ /* Channel Configuration Error */ Error_Handler(); } ADC->CCR &= ~ADC_CCR_VBATE;}uint8_t GetTempValue(float *TempValue_degC) {
unsigned short int count;
uint32_t Adc_Value =0; uint32_t Adc_Value2 =0; float vsense=0; float samples =0; float Temp; TempINIT(); for(count=0;count<20;count++) { HAL_ADC_Start(&AdcHandle);if (HAL_ADC_PollForConversion(&AdcHandle, 1) == HAL_OK) {
Adc_Value = (uint16_t)HAL_ADC_GetValue(&AdcHandle); Adc_Value2 =Adc_Value; samples+=Adc_Value; } else { Adc_Value = 0; return ERROR; } HAL_ADC_Stop(&AdcHandle); } samples = samples/20; vsense = ((samples)*(3300))/4096;Temp = (((vsense) - (760))/(2.5)) + 25; *TempValue_degC = Temp; Adc_Value = 0; samples = 0; return SUCCESS;}/**
Thanks In Advance
with regards,
Himasagar.