Skip to main content
Rakesh Yedri
Visitor II
July 13, 2017
Question

Surge Test Failure

  • July 13, 2017
  • 0 replies
  • 845 views
Posted on July 13, 2017 at 06:50

Dear Team,

Please find the attached design. ehg7520_cpu_ board.pdf 

In my product design i have used TVS diodes and ORing diodes from ST Micro electronics. My product has to under go the following test. TEST_Cases.xls .

Our input voltage range is from 12V to 57Vdc. Dual supply (DC_1 & DC_2).

During the surge test the DUT(Device under test) was failing. We are observing the power cycling issue. Please suggest us the solution.

Note: With 12V input my test passed but with 48V input it fails. Some observations are attached as Surge test report.

egards,

Rakesh

+91-9481421422

mailto:rakesh.y@atop.in

ATOP COMMUNICATION SOLUTIONS PVT LTD,

#surge-test
This topic has been closed for replies.