Question
Problem to reach high Frequency on GPIO
Posted on August 25, 2017 at 16:34
Hi,
i'm using stm32 nucleo board. The oscillator is configured to 32MHz speed.
Now, if i use the easy following code in the main:while(1)
{
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, 1);
HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, 0);}
the frequency i measure on the LD2 pin is only 750KHz. This is really strange, i expect
to run more quick than 750KHz only.Can someone help me?