Skip to main content
Lei Sun
Associate II
July 28, 2017
Question

Test SPI on STM8S value line discovery evaluation board

  • July 28, 2017
  • 0 replies
  • 1096 views
Posted on July 28, 2017 at 23:12

hi, I want to test the SPI function on the STM8S value line discovery evaluation board. I only have this EVB and some cables, LEDs. Is it possible to make some simple test of the SPI function, such as communicating between this EVB and PC without extra hardware. I have found many examples, but all of them need some extra hardware, such as LCD, MAX72XX LED array, etc. Is it possible to only use this EVB and PC? Thanks a lot.

Bo

#spi #stm8s
This topic has been closed for replies.