Skip to main content
ellie wang
Visitor II
July 24, 2017
Question

I2C communication with PN532

  • July 24, 2017
  • 0 replies
  • 1355 views
Posted on July 24, 2017 at 13:07

hi !

I tried to connect STM32F103VET6 to NFC reader (PN532). As I read in pdf documentation of PN532 User Manual, i choose to use I2C. I didn't use the library of  I2C, just use two GPIOs to analog the I2C communication protocol. The question is  i didn't find the precise sequence diagram in the pdf. 

In the pdf ,the following figure depicts the mechanism:

1. command sent by the host controller

2. the host controller polling the status byte

3. ACK frame sent by PN532

4.

the host controller polling the status byte

5. RESPONSE

 frame sent by PN532

since i use the analog 

I2C communication protocol, the precise seqence diagram is very important to programming. 

I tried so many times and It doesn't work . May be there is something wrong..

Thank-you, see you on community.

    This topic has been closed for replies.