Solved
STM32CubeMX FreeRTOS and __weak
Posted on September 13, 2017 at 14:49
When enabling the FreeRTOS idle hook STM32CubeMX generates a function with the following prototype in the freertos.c file:
__weak void vApplicationIdleHook( void )
However __weak isn't defined in any one of the included header files (I'm using GCC with Makefile target) so the file can't be compiled until defining the __weak as __attribute__((weak)) somewhere.
#idle-hook #freertos