Skip to main content
After Forever
Senior III
September 14, 2017
Solved

STM32CubeMX v4.22.1 Custom Firmware Location in the IOC file

  • September 14, 2017
  • 1 reply
  • 839 views
Posted on September 14, 2017 at 10:41

I have the 'Use Default Firmware Location' checkbox set in the 'Project Settings' window but nonetheless my firmware location path is being saved in the IOC file when I save it:

...
ProjectManager.CustomerFirmwarePackage=/home/jive/stm32/repository/STM32Cube_FW_L0_V1.0
...�?�?�?

I think it would be better not to save the custom firmware location when the default location checkbox is set because different developers sharing the same IOC file in the version control system have different default repository paths.

    This topic has been closed for replies.
    Best answer by Jeanne Joly
    Posted on February 05, 2018 at 15:38

    Hi

    sweden

    ,

    Thanks for your suggestion.

    When the specification was written, we decided to keep the FW path even if the user chose his ownpath or else he wouldneed to re-enter the path each time he re-generated his project.

    I fully understand your point but we chose to write the user path in the generated ioc (if someone uses the generated ioc and needs to change the path, he can do it manually by editing the ioc file) instead of deleting the path (in this case, everybody would have to write their own paths and I'am pretty sure we would have many complaints...).

    I hope your understand our choice.

    Don't hesitate to have a look to this doc

    http://www.st.com/content/ccc/resource/technical/document/user_manual/10/c5/1a/43/3a/70/43/7d/DM001047pdf/files/DM001047pdf/jcr:content/translations/en.DM001047pdf

    for further details (paragraph 5.8.1 for the default FW location).

    BR. Jeanne

    1 reply

    Jeanne Joly
    Jeanne JolyBest answer
    Associate
    February 5, 2018
    Posted on February 05, 2018 at 15:38

    Hi

    sweden

    ,

    Thanks for your suggestion.

    When the specification was written, we decided to keep the FW path even if the user chose his ownpath or else he wouldneed to re-enter the path each time he re-generated his project.

    I fully understand your point but we chose to write the user path in the generated ioc (if someone uses the generated ioc and needs to change the path, he can do it manually by editing the ioc file) instead of deleting the path (in this case, everybody would have to write their own paths and I'am pretty sure we would have many complaints...).

    I hope your understand our choice.

    Don't hesitate to have a look to this doc

    http://www.st.com/content/ccc/resource/technical/document/user_manual/10/c5/1a/43/3a/70/43/7d/DM001047pdf/files/DM001047pdf/jcr:content/translations/en.DM001047pdf

    for further details (paragraph 5.8.1 for the default FW location).

    BR. Jeanne