Skip to main content
Jason Jin
Associate II
August 14, 2017
Solved

Why the commutation delay doesn't work

  • August 14, 2017
  • 2 replies
  • 1854 views
Posted on August 14, 2017 at 07:31

Greetings,

I generate the project using 

0690X00000607qIQAQ.png

To control the bldc motor with hall sensors interface. The configuration is as below:

0690X00000607fWQAQ.png

Refer to TIM4, which is set as the hall sensor interface, the detail configuration is as below:

0690X00000607sEQAQ.png

Refer to TIM1, which is set as the PWM-generated interface, the detail configuration is as below:

0690X00000607rGQAQ.png

After my debug, the motor can be driven. But I found the commutation delay doesn't work at all. So can anyone explain what the commutation delay means? Which event would affected by this delay setting? Why this delay doesn't work? I measured between Hall sensor input and TIM1_TRG_COM_TIM11_IRQHandler(), and I also measured between 

TIM1_TRG_COM_TIM11_IRQHandler() and HAL_TIMEx_CommutationCallback(). No delay is related to this setting.

B.R.

Jason

#bldc-commutation-delay #stm32cube
This topic has been closed for replies.
Best answer by Jason Jin
Posted on August 15, 2017 at 06:53

0690X00000607ruQAA.png 0690X00000607snQAA.png

2 replies

Jason Jin
Jason JinAuthor
Associate II
August 15, 2017
Posted on August 15, 2017 at 06:51

I would like to update the progress. I have found the root cause. It caused by STM32CubeMX tools. TIM1 shall be set as the slave timer while TIM4 shall be set as the master timer with OC2REF to TRGO. I wish ST guys would fix the bugs to let function of commutation delay go.

B.R.

Jason 

Jason Jin
Jason JinAuthorBest answer
Associate II
August 15, 2017
Posted on August 15, 2017 at 06:53

0690X00000607ruQAA.png 0690X00000607snQAA.png