Skip to main content
Andy Zh
Associate
August 11, 2017
Question

Vibration measurement sensors

  • August 11, 2017
  • 3 replies
  • 1120 views
Posted on August 11, 2017 at 10:20

Dear,all:

      ST companies have used for vibration measuring acceleration sensor? Requirements are as follows:

Frequency response: more than 1kh

Range: 0-40 g

Power:Low power consumption

Used in water pump, fan and other industrial sites

     if ST companies have not these sensor,Can you introduce other company sensor?

This topic has been closed for replies.

3 replies

ST Employee
August 14, 2017
Posted on August 14, 2017 at 11:22

You can consider

http://www.st.com/content/st_com/en/products/mems-and-sensors/accelerometers/h3lis331dl.html

 the range is 100/200/400g, but the maximum output data rate is only 1kHz.

Are you sure you need to measure vibration up to 40g? If 16g would be enough you can also consider

http://www.st.com/content/st_com/en/products/mems-and-sensors/accelerometers/iis2dh.html

 which is capable to provide data with output data rate up to 5376 Hz.