Skip to main content
Oktay TURK
Associate
April 28, 2018
Question

STM32F103 Maximum input Frequency

  • April 28, 2018
  • 1 reply
  • 725 views
Posted on April 28, 2018 at 19:09

I use STM32F103 how much is the maximum input maximum encoder frequency. For example if the possible i reading the 20 KHz. I use the TIMER4 encoder mode but i not read the up the 2 KHz. How much is the maximum frequency value?

    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    April 28, 2018
    Posted on April 28, 2018 at 20:14

    The TIM's should work into the MHz, but don't expect to interrupt at such high rates.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..