Skip to main content
ANNU CHERIAN
Associate II
August 18, 2017
Question

How to achieve maximum system clock (168MHz) in stm32f446zet

  • August 18, 2017
  • 5 replies
  • 1341 views
Posted on August 18, 2017 at 06:47

RCC->APB1ENR |= (1<<28);

PWR->CR |= (PWR_CR_VOS);

               

RCC->CR |= (1<<0);

RCC->CR |= (RCC_CR_HSICAL_4);                                   //

Internal high-speed clock calibration

RCC->CFGR |= RCC_CFGR_SW_HSI;                              //

HSI oscillator selected as system clock

RCC->CFGR |= RCC_CFGR_PPRE2_DIV2;                      //

APB high-speed prescaler (APB2)

RCC->CFGR |= RCC_CFGR_PPRE1_DIV4;                      //

APB Low speed prescaler (APB1)

RCC->CFGR |= RCC_CFGR_HPRE_DIV1;                        //

AHB prescaler

RCC->CR &= ~(1<<24);                                                       // 

PLL OFF

RCC->PLLCFGR &= ~(1<<22);                                           //

HSI clock selected as PLL

RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLM;        

RCC->PLLCFGR |= RCC_PLLCFGR_PLLM_4;                  //

Division factor for the main PLL (PLL) input clock (16)

RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLN;             

RCC->PLLCFGR |= RCC_PLLCFGR_PLLN_4;                  //

Main PLL (PLL) multiplication factor for VCO (336)

RCC->PLLCFGR |= RCC_PLLCFGR_PLLN_6;

RCC->PLLCFGR |= RCC_PLLCFGR_PLLN_8;          

RCC->PLLCFGR &= ~RCC_PLLCFGR_PLLP;                

RCC->PLLCFGR |= RCC_PLLCFGR_PLLP_1;                 // Main PLL (PLL) division factor for main system clock(2)

RCC->CR |= (1<<24);                                                         // enable PLL       

while(!(RCC->CR & RCC_CR_PLLRDY));                       // waiting for PLL lock

RCC->CFGR |= RCC_CFGR_SW_PLL;                           // PLL_P selected as system clock

Above code shows configuration to achieve maximum system clock (168MHz) , but during running time on keil uvision5 compiler  shows 'cannot access memory' . Please suggest a method to solve this issue .......

#stm32f446-system-clock
This topic has been closed for replies.

5 replies

Jan Waclawek
Visitor II
August 18, 2017
Posted on August 18, 2017 at 12:56

Are you sure Keil's complaint is related to these lines? Are you trying to access external memory with the debugger? (I don't use Keil so these are blind shots)

JW

Tesla DeLorean
Guru
August 18, 2017
Posted on August 18, 2017 at 16:01

Yikes! That's hideously inefficient code, thought the point of this level of programming was to be minimal/optimal.

You'll need wait states for the FLASH

You'll want to avoid errata/hazards of enabling clocks and immediately touching the same peripheral.

Bunch of assumptions about initial conditions.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ANNU CHERIAN
Associate II
August 19, 2017
Posted on August 19, 2017 at 09:05

This code work for system clock upto 142MHz by changing the value of PLL_N . On increasing further, error 'Cannot access memory' arises.

I am using STM32F446 Nucleo 144 Board.

Tesla DeLorean
Guru
August 19, 2017
Posted on August 19, 2017 at 14:27

{

  uint32_t pll_n = 360, pll_p = 2, pll_m = 16, pll_q = 7, pll_r = 7;

  RCC->APB1ENR |= RCC_APB1ENR_PWREN;

  RCC->CFGR |=  RCC_CFGR_HPRE_DIV1  | /* HCLK = SYSCLK / 1*/

                RCC_CFGR_PPRE2_DIV2 | /* PCLK2 = HCLK / 2*/

                RCC_CFGR_PPRE1_DIV4;  /* PCLK1 = HCLK / 4*/

  /* Select regulator voltage output Scale 1 mode, System frequency up to 168..180 MHz */

  PWR->CR |= PWR_CR_VOS;

  /* Configure the main PLL */

  RCC->PLLCFGR = pll_m | (pll_n << 6) | (((pll_p >> 1) - 1) << 16) |

                   (RCC_PLLCFGR_PLLSRC_HSI) | (pll_q << 24) | (pll_r << 28);

  RCC->CR |= RCC_CR_PLLON; /* Enable the main PLL */

  while((RCC->CR & RCC_CR_PLLRDY) == 0); /* Wait till the main PLL is ready */

  /* Enable the Over-drive to extend the clock frequency to 180 Mhz */

  PWR->CR |= PWR_CR_ODEN;

  while((PWR->CSR & PWR_CSR_ODRDY) == 0);

  PWR->CR |= PWR_CR_ODSWEN;

  while((PWR->CSR & PWR_CSR_ODSWRDY) == 0);

  /* Configure Flash prefetch, Instruction cache, Data cache and wait state */

  FLASH->ACR = FLASH_ACR_ICEN | FLASH_ACR_DCEN |

    FLASH_ACR_PRFTEN | FLASH_ACR_LATENCY_6WS; // 5WS Might work

  /* Select the main PLL as system clock source */

  RCC->CFGR &= (uint32_t)((uint32_t)~(RCC_CFGR_SW));

  RCC->CFGR |= RCC_CFGR_SW_PLL;

  /* Wait till the main PLL is used as system clock source */

  while ((RCC->CFGR & (uint32_t)RCC_CFGR_SWS ) != RCC_CFGR_SWS_PLL);

}
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ANNU CHERIAN
Associate II
August 24, 2017
Posted on August 24, 2017 at 08:47

Thank You Clive .Maximum clock frequency (180MHz) achieved when enabling over drive and FLASH .