Skip to main content
BG1
Associate III
December 4, 2017
Solved

While loop stucks

  • December 4, 2017
  • 23 replies
  • 3462 views
Posted on December 04, 2017 at 18:21

Hello ..

I am having a very weird issue with my code piece ..

The MCU is STM32F407VET6 .. What I'm trying to do is sending a string via USART1 peripheral module .. In order check if the character in the USART1 is sent out of the USART1->DR register I am continuously checking the 'Transmit Complete Bit of the usart1 status register

The code below works well ...

TC1 is defined as USART1_SR_TC register bitband alias ...

#define TC1 *((uint32_t *)(0x42220018)) //Previously defined at the top of the main file

void EXTI4_IRQHandler(void)

{

uint8_t i;

char x[6]='BURAK\n';

EXTI_PR_Bit4=1; // Cleared by writing 1

// ISR code

TC1=0;

for(i=0;i<7;i++)

{

USART1->DR=x[i];

while(!(USART1->SR&USART_SR_TC));// Transmit Complete ?

}

TC1=0;

}

BUT !

When I replace

while(!(USART1->SR&USART_SR_TC));

with

while(TC1==0);

The code stucks.. freezes ... and stops ...Why does it happen ?? Are Bit-Band Aliases not reliable things to use with while ,if , for statements ?? Does it have to be read/modify/write sequence always ??

Thanks in advance ..

#flag-check #bitband #while #stuck

Note: this post was migrated and contained many threaded conversations, some content may be missing.
    This topic has been closed for replies.
    Best answer by waclawek.jan
    Posted on December 04, 2017 at 18:39

    #define TC1 *((volatile uint32_t *)(0x42220018))

    23 replies

    waclawek.jan
    waclawek.janBest answer
    Super User
    December 4, 2017
    Posted on December 04, 2017 at 18:39

    #define TC1 *((volatile uint32_t *)(0x42220018))

    BG1
    BG1Author
    Associate III
    December 5, 2017
    Posted on December 05, 2017 at 06:52

    I tried the volatile add-on with STM32F303RET6 and It failed .. But It solved my problem with STM32F407VET6 ... Thank you so much :.

    Tesla DeLorean
    Guru
    December 4, 2017
    Posted on December 04, 2017 at 18:40

    Don't look at the registers in the debugger.

    Use TXE to see if the register is EMPTY first, rather than waiting for TC afterward, as that is the slowest way to do it.

    Avoid looping in IRQ Handler for thousands of micro-seconds.

    Bit-banding is not recommended for peripheral registers, it's not atomic and can have side-effects. Especially TIM->SR

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    ChrisH
    Associate III
    December 4, 2017
    Posted on December 04, 2017 at 19:22

    Turvey.Clive.002

    could you recommend any good article on bit-banding when working with registers? I would like to know how to safely do it, I know there is a feature on CortexM3/M4 which allows mapping mem regions in order to have an atomic operation.

    Tesla DeLorean
    Guru
    December 4, 2017
    Posted on December 04, 2017 at 20:30

    You can have mostly atomic access to memory, no good for peripherals as they can change state during RMW action.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Andrew Neil
    Super User
    December 5, 2017
    Posted on December 05, 2017 at 20:14

    Cross post - on Keil forum: 

    http://www.keil.com/forum/63180

     
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    BG1
    BG1Author
    Associate III
    December 7, 2017
    Posted on December 07, 2017 at 12:22

    Define the 'Cross Post' ! ??

    A topic on the same http address and domain ? or even different ? Please stay out of the topics if you really don't want to contribute !

    Andrew Neil
    Super User
    December 7, 2017
    Posted on December 07, 2017 at 12:30

    Yes, a 'Cross-Post' is posting the same question in multiple places.

    It is considered impolite because you end up wasting people's time as they give an answer in one place, unaware that someone else has already given the same answer elsewhere.

    If you are going to cross-post, then always give links between the posts, and be sure that you keep monitoring all locations!

    https://en.wikipedia.org/wiki/Crossposting

     
    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.