Question
Reliable U(S)ART between two STM32 MCUs with internal oscillator
Posted on September 15, 2017 at 11:37
Hello!
I have a best practice question.
Correct UART communication requires the transmitter and receiver clocks differ by less than 5% (2.5% per MCU), otherwise communication errors may occur. For the temperature range TA = 0 to 85°C the Accuracy of the HSI oscillator is good enough. But for temperatures below 0°C, the HSI has too less accuracy.
What do you do?
• Use external oscillator• Use autobaud detection.• Oscillator calibration with external signal• Do not care• ….