Skip to main content
Thai Le
Associate
August 23, 2017
Question

Set up B-L072Z-LRWAN1, send data to multitech gateway and loriot

  • August 23, 2017
  • 3 replies
  • 1062 views
Posted on August 23, 2017 at 09:02

Hello, currently im using B-L072Z-LRWAN1 send AT command to multitech gateway and server is loriot.io. And i cant get data at the server.

Here some information:

Firmware version B-L072Z-LRWAN1 v1.1.1

AT command:

   AT

   AT+CFM=0

   AT+NJM=0

   AT+DADDR=...

   AT+NWKSKEY=...

   AT+APPSKEY=...

   AT+JOIN

   AT+NJS=? (response = 1)

   AT+SEND=1:0123

   OK

   txDone

   rxTimeOut

   rxTimeOut

I cant connect to Multitech gateway.

Any suggestion?

#lora #b-l072z-lrwan1
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
August 23, 2017
Posted on August 23, 2017 at 15:14

There is a problem with the sscanf() in the AT+SEND command parsing

https://community.st.com/0D50X00009XkXrMSAV

 

uint8_t appport; needs to be 

uint32_t appport;

See also the rest of that thread for some foundation in the issue.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Thai Le
Thai LeAuthor
Associate
August 23, 2017
Posted on August 23, 2017 at 15:22

Thank for fast answer Clive One

I will try it tomorrow, but my config above is correct ?

I see when i run AT+JOIN the DADDR, 

NWKSKEY, APPSKEY is back to default. Is there something wrong?

Tesla DeLorean
Guru
August 23, 2017
Posted on August 23, 2017 at 16:57

I'm doing mostly point-to-point communication, I don't have a Gateway to tinker with.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..